AXIS#.VL.ERR

Description

AXIS#.VL.ERR is the velocity loop error. It is calculated in the velocity loop as the difference between AXIS#.VL.CMD and AXIS#.VL.FB .

Versions

Action Version Notes
Implemented 02-00-00-000

General Information

Type

Read Only

Units

Rotary: RPM, RPS, deg/s, (custom units)/s, rad/s

See Velocity Units for details.

Range

N/A

Default Value

N/A

Data Type

Float
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
AXIS1.VL.ERR

5011h

05h

Signed32

Velocity

-

Read only

Yes

AXIS2.VL.ERR

5111h

05h

Signed32

Velocity

-

Read only

Yes

EtherNet/IP

Name

ID

Hex

Data Type

Access

Units

AXIS1.VL.ERR

6023

1787

Signed32

Read Only

Velocity

AXIS2.VL.ERR

71559

1178

Signed32

Read Only

Velocity

PROFINET

Parameter

PNU

Data Type

Access

Units

AXIS#.VL.ERR

6023

Float

Read Only

Velocity